EGEAR.RATIO
Description
Ratio must be set more recently than EGEAR.PULSESIN or EGEAR.PULSESOUT in order to use EGEAR.RATIO to control electronic gearing.
General Information
|
Type |
TBD |
|
Units |
Motor revolutions / Encoder Revolution |
|
Range |
-2,000 to 2,000 |
|
Default Value |
1 |
|
Data Type |
Float |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1074 |
No | 32 bit | No |
M_01-05-11-000 |
Related Topics
EGEAR.ON | EGEAR.PULSESIN | EGEAR.PULSESOUT | FB2.SOURCE | FB2.ENCRES | FB2.MODE